Part Number: TS3USB221
Tool/software:
Hi,
I have designed a device which takes 1 USB input and allow me to switch between two USB outputs.
The board i designed right now is not working at all. It has only one problem at a moment as i connected the D+ line to D- line on the IC. Connections at the connectors are quite OK.
However for better routing I thought to connect D+ line to D- of IC and vice versa.
Do you guys think it will be an issue if D+ goes through D- line of IC ?
Stack up and impedance profile is OK as i have designed many boards based on same impedance profile of 90 ohms and everything works well in other designs. So diff impedance is not an issue at all.
Any help shall be appreciated.
Regards.