Part Number: DS250DF410
Tool/software:
In the Data Sheet, I see that "Each" Differential Rx Input has a 100Ohm Termination:

In the Pin Function Description is states the following:

The Receiver Input Specifications are also shown:

Question-1: What is the Receiver Input Common Mode Range {I see "Maximum" Vid = 1225mVppd}?
Question-2: If I'm injecting a Clock at 1.611328125GHz in one of the Rx Ports in order to Generate PRBS at its corresponding Tx Ports, is AC Signal Detection Relevant {Does 1.6GHz Clock Amplitude need a "Specific" Level}?
Note: I see 192mVppd "Minimum" Vsdat required to "Assert" Signal Detection at Rx Ports and 147mVppd "Maximum" Vsddt required to "De-Assert" Signal Detection at Rx Ports