Part Number: SN65HVD485E
Tool/software:
I would like to inquire about the label show d/c 2309 , the lower left is 33, but the tape reel is sorted 33 and 34 not in order, and laser marks vary in thickness, is this normal?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD485E
Tool/software:
I would like to inquire about the label show d/c 2309 , the lower left is 33, but the tape reel is sorted 33 and 34 not in order, and laser marks vary in thickness, is this normal?


Hi Howard,
See comments below:
"The A/T site date code is when the material got marked. So if its end of a month/start of next month, the marking on that lot will be 32 or 33(just an example) if it got processed over 2 days.
While testing, the units from both days (32 and 33 marking) will be all together without any order; and based on what got to test first, they will be arranged in the T&R accordingly.
The marking variation is probably due to different machines usage. They both should still be within spec."
Based on this, it seems like these kind of variations are okay.
-Bobby