Part Number: DS90UB662-Q1
Other Parts Discussed in Thread: DS90UB962-Q1
Tool/software:
Hi team,
Please could I ask for your help to select the correct device for a camera aggregation system. The end customer is Iveco, where they have a requirement to be able to connect 4x camera as described.
The CDC shall support the following characteristics for the digital inputs:
- DES compatible with the 933 SER
- DES to support 1MP @ 60fps or 2MP @ 30fps for all digital inputs. Example 936, 954.
- As nice to have, DES with support for higher resolutions (2 or 3MP @ 60fps). Example 960, 9722.
- Format used from MY24 cameras is YUV422 10bits
Visteon are limited due to the number of CSI-2 interfaces on their SoC, so ideally using one 4-lane CSI interface for the DES.
Help with the calculations of the per-lane FPD rates, and thus the CSI aggregated data rate would be great to have.
BR, Ross