This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VAR-3P-SOM-AM62: What is the maximum frequency for events to be correctly timestamped via HW-TS-PUSH in CPTS?

Part Number: VAR-3P-SOM-AM62
Other Parts Discussed in Thread: AM625

Tool/software:

Hello,

hardware time stamps (HW-TS-PUSH in CPTS ) are intended to be an extremely low frequency signals. What is the maximum accepted frequency of these signals for AM625?

BR

Zain

  • Hello Zain,

    From the hardware perspective, you can find details about the required waveform characteristics from the AM62x datasheet, section "Timing and Switching characteristics" > CPTS.

    I am not sure exactly what you are asking for ("low frequency" usually refers to pulses that occur more slowly, like a 1kHz signal, while "maximum frequency" usually refers to pulses that occur more quickly, like a 1GHz or 1MHz signal). Feel free to reply with more information about what kind of pulse you are looking to measure.

    Regards,

    Nick