Part Number: DS90UB960-Q1EVM
Tool/software:
i want to connect and HDMI capture card to this DS90UB960-Q1EVM board Can i use a MIPI-to-HDMI bridge to connect my HDMI capture card to it ? (link to bridge:www.digikey.ca/.../7623050
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1EVM
Tool/software:
i want to connect and HDMI capture card to this DS90UB960-Q1EVM board Can i use a MIPI-to-HDMI bridge to connect my HDMI capture card to it ? (link to bridge:www.digikey.ca/.../7623050
Hi Arseniy,
Are you sure this is a bridge to convert MIPI CSI-2 to HDMI? If that is the case, then you may use it if you can connect the CSI-2 onboard connector via wires to this bridge adapter.
Its the only one ive been able to find. I thought you just clip it on and its good to go.
I am not aware of an off-the-shelf solution. Customers have been designing their own hardware.
Also, I have seen some people using the Raspberry pi to convert MIPI CSI-2 to USB, but nothing to HDMI.
You may need to look buy a cable which can be connected between the UB960 EVM's CSI-2 connector and the Raspberry pi. Unfortunately, I have no suggestions here since we never used this use-case.
I have seen other customer develop their own adapter board to interface between the EVM's CSI-2 connector and the Raspberry pi.
what can be used to get these outputs now, it seems like there are no 40 pin cables