Part Number: DS90UB928Q-Q1
Tool/software:
hi expert,
could you help provide the spec of the delay from video input to output for DS90UB928
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB928Q-Q1
Tool/software:
hi expert,
could you help provide the spec of the delay from video input to output for DS90UB928
Hi Colt,
Video latency calculations are explained through this E2E regarding timings and typical DES delays:
Please let me know if this answers your question, or if you need further clarification.
Best!
Miguel
Hi Qiang,
Since you are unable to see the internal forum, I will provide the brief explanation here:
The SER should buffer 1-2 video lines before starting transmission under typical conditions, DES can buffer up to 512 pixels.
Typical latency = 1 * line time + 512 pixel time
Here is an example calculation:
Active Video Timing = 3840 x 2160 @ 60 fps
Total Dimensions = 4000 x 2222
PCLK = 533.25 MHz
Pixel Time = 1/533.25 MHz = 1.87 ns per pixel
Line Time = 1.87 ns * 4000 px = 7.48 µs (total horizontal represents one line buffer)
Typical latency = 1 * 7.48 µs + (512 * 1.87 ns) = 8.437 µs
Please let me know if this explains what you are looking for, or if further clarification is needed.
Best,
Miguel
You're welcome!
Feel free to mark this thread as resolved if this is all you needed! :)