Part Number: TCAL9539-Q1
Other Parts Discussed in Thread: TMAG5173-Q1, , TCAL9539
Tool/software:
Hello,
We are using multiple TMAG5173-Q1 and a single TCAL9539-Q1 IC on the same I2C bus in our project. If we start the measurement simultaneously on all sensors using the General Call Write, would this cause any operational issues with the TCAL9539, which is also connected to this bus?

I was redirected from the sensor forum to the interface forum to check whether the TCAL9539-Q1 is affected by I2C General Write. I am adding my previous question as a related inquiry.
Additionally, I have attached the related section from the datasheet of TCAL9539-Q1.

Best regards,
Egemen