Part Number: TCAN4550
Tool/software:
Hi,
When the surface temperature of the IC reaches 50°C or higher, the CAN signal is not output and bit errors occur.
At this time, the oscillator output is connected to OSC1 and OSC2, but no load capacitance is implemented. The bit error problem was solved by connecting a 10pF capacitor in parallel.
Could you please tell me what possible internal operation may be causing TCAN4550 bit errors due to temperature dependence?
Is it possible that the parasitic capacitance inside the IC changes as the temperature rises, causing the clock mode to change?
Best Regards,
Nishie