Tool/software:
Hello, is it possible to connect DS90UB960-Q1EVM board to the reComputer J30. The board has 2 MIPI CSI Outputs. The J30 reComputer contains MIPI-CSI connector which is 22 pin. Is there a wire that can be used to connect both of these together ? the MIPI CSI output on the board is 40 pin