Tool/software:
Hi team,
we want to change from TCAN1057ADRQ1 to a Grado 0 part being TCAN1057AEVDRQ1.
Instead of pin 5 being NC the grade 0 part has a Vio pin. This has to be tied to the IO voltage of the MCU to my understanding, right?
So if in my system the MCU only has 5V input it should also have 5V IO levels and if the TCAN1057AEV-Q1 is powered by the same 5V, we just tie Vio to Vcc.
Best
Khai