This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB522P:

Part Number: TUSB522P

Tool/software:

Hello,

I have a related question about cascading USB redrivers. Please refer to the image below. There is already a USB redriver that has been implemented on the SBC card in one of the backplane slots. The USB3.0 signal has to travel several inches on the backplane and the Front IO board via an interface connector and then to the outside world via the Amphenol USB Type-A connector. I'd like to add another redriver, namely TUSB522P, on the IO board right before the Amphenol connector. Would just having two redrivers cause a jitter issue? I'd like to use a redriver rather than a retimer for it is less complex to use.

Does TI offer any USB retimers?  

Thank you for your help.

Ray

/cfs-file/__key/communityserver-discussions-components-files/138/Redriver-Q.pdf