Part Number: TUSB1004
Tool/software:
Hi team
They want to use the device for USB3.2, 5Gbps, but they just need 1 port, though the deivce has 2 ports. So they have questions below. Could you support this?
- Can they use either port 1 or port 2 for USB3.2, 5Gbps? Are there any differences between port 1 and port 2?
- Could you tell the way to deal with unused pins for the unused port?
- Could you tell smaller-size redirver? The size of the device is large for their system.
Regards,
Noriyuki Tkahaashi