Part Number: SN75176A
Other Parts Discussed in Thread: SN65LBC176, THVD1520,
Tool/software:
I am working at fault finding a system where an SN75176AP stops working when ambient temperature is around 50°C.
System setup
Isolated RS485 with the SN75176AP transceiver driven by a 9600 baud half duplex link. Cable length approx 1200 meter. 2 wire only. Isolated grounds not connected.
Boards mounted in a sealed aluminium enclosure for deep water immersion.
Leaving the electronics on and allowed to warm up in an ambient temperate between 30 and 35°C, the internal temperature rises and eventually the link stops working.
Opening the enclosure and the part cools down and starts working again. Apply gentle heat to the SN75176 area only and after it heats up to about 50 deg (observed on a thermal camera), the link stops working. Cool the SN75176 with a cold blast from an air dust cannister and the part starts working and data connection resumes. This is repeatable, heat, stops working, cool, comms resumes.
I don't think that temperature is a direct effect as the device is specified for 0-70°C rating. I suspect there is some common mode voltage causing further heating although I was not able to measure this at the time.
Any idea what's going on?
My next step is to build a test circuit and find an alternative device with a wider operating range and higher common mode voltage tolerance.