Part Number: TRS3221E
Tool/software:
Hi,
I'm using TRS3221EIRGTR and it works well until baud rate of 115200, but fails - data corruption - on 230400, though it's specified until 250Kbps (I'm using TRS3221EIRGTR).
This is the schematics:

The UART_RX_TA and UART_TX_TA are at 1.8V levels.'
TB_RS232_RX and TB_RS232_TX are routed to a connector.
Please kindly advice.
Thanks,
Matan