Part Number: TCA9509
Tool/software:
Hi,
i'm using the part in order to buffer the I2C line going to a sensor out from board. but i use it also to on-board device which i connected directly to the MCU without buffering.
i read in the datasheet that pullups in the A side are not allowed? i didn't understand if not allowed or not needed?
the problem is that I thought to disable the buffer whenever the external sensor is not in use. and then i won't have the 1mA current source active, is that true?
so can i connect pullups to the A side or not?
all sides uses the same 3.3V voltage.
pls see the diagrem:
my question is about the circled resistors.
Thanks,
Israel