This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: The max value of Input capacitance to Ground (CANH or CANL)

Part Number: TCAN1145-Q1

Tool/software:

Dear all:

         In the datasheet of TCAN1145, there is "Input capacitance to Ground (CANH or CANL)" , and the max value of it is 20pF

         Could I konw which CAN transceiver could meet the requirement that max value of input capacitance to Ground (CANH or CANL) is below 20pf ?

regards

Hongyi Zhuang

  • Hongyi,

    The typical measured value of our CANH and CANL pin capacitance is closer to 12-15pF, but it could be a maximum of 20pF. We do not have any other transceivers with lower pin capacitance.

    Regards,

    Eric Hackett