This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB936-Q1: EQ level vs insertion loss suggestion

Part Number: DS90UB936-Q1

Tool/software:

hi team,

Could you suggest a suitable EQ level? Customer would like to change the AEQ_min and AEQ_max to improve the link robustness and avoid EQ lock to a wrong level.

We are running the MAP to get some guidance, at the same time, pls check are there any 93x/95x insertion loss vs EQ suggestion table available to make a comprehensive decision of EQ setting.

- 935+936 sync mode with 4Gbps fpd-rate

- EE is E-mirror application with 10m coax cable

- Insertion loss test result as below -15db@2Gbps

Regards,

Dongbao