Part Number: SN65DPHY440SS
Tool/software:
Hello,
I would like to use SN65DPHY440SS between MIPI DSI type LCD screen and a micro controller, to improve signal integrity.
I would like to implement a SN65DPHY440S between the MPU and the Driver IC of my LCD.

I have a couple a question,
- Can we use the SN65DPHY440SS WITHOUT the I2C interface of the device. I will implement either pull up or pull down on the VSADJ_CFG0 & EQ/SCL & ERC/SDA & PRE_CFG1
- The SN65DPHY440SS has the bidirectional LP mode supported, but i don't understand how it is set.
Thanks in advance for any hint.
Regards.