This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6E001: Continuous current rating of diodes to positive supply

Part Number: TPD6E001


Tool/software:

What is the continuous current rating for the diodes between the input signal and the supply rail for the TPD6E001?

For context, when using the TPD6E001 for ESD protection of an RS-422 receiver, there is a possibility a remote driver could be powered when the receiver is not. In this scenario the high-side ESD diode allows the power rail of the receiver to be back-powered, and the remote RS-422 driver will source the current.

For this condition a return or reference connection exists between the driver and receiver in the form of cable shields where local references (GNDs) are connected to the shielded enclosures. For cabling not exceeding 40 feet, the common reference potential suggests minimal common mode voltage between the driver and receiver. 

While the usage of the TPD6E001 in this application is questionable, and possibly not recommended, knowing the permissible continuous current is needed.