Tool/software:
Hi TI CAN Expert,
Currently I am considering the worst CAN topology using TCAN1462-Q1 (with SIC) like below:
- CAN FD frame
- One master #0 connected with 6 branches in parallel
- Each branch has 6 CAN node (#1~#6, each branch can be considered as linear topology)
- Each branch max total distance from #0 to #6 is 20 meters
- Typical data rate: 2Mbps (max to support 5Mbps if possible)
- The communication only happen from #0 to #1-#6, or from #1-#6 to #0. One branch won't talk to other branch.
Physical connection:
- For #0, there are 6 connectors for cable, and each connector is connected in parallel to CANH/CANL. There is no gateway there, only one CAN transceiver with termination.
- For #1-#6, there are 2 connectors for cable, and each connector is connected in parallel to CANH/CANL
My questions:
- Does this topology make sense to you? And for this topology, how to design the termination network?
- Does TI has any tool to simulate the topology and any way to improve it?
Looking forward to your feedback!



Regards
Nic