This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822H: Must TPI termination supply voltage be 3.3V

Part Number: DP83822H

Tool/software:

From the DP83822 datasheet, it says to connect center tap to AVD supply, either 1.8V or 3.3V

But if i use AVD=1.8V, do i still need to connect termination to 3.3V supply?

According figure 9-2 it seems so, but is this true?