Part Number: SN65DSI85Q1-EVM
Tool/software:
The customer want to do the validation using our EVM, but there is no connecting wire for them.
Can you share the connecting wire name for the below two block? Or whether the customer could buy it?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DSI85Q1-EVM
Tool/software:
The customer want to do the validation using our EVM, but there is no connecting wire for them.
Can you share the connecting wire name for the below two block? Or whether the customer could buy it?

Hi Fabio,
In the EVM user guide, the "2.1 Connectors for DSI8X Input Ports" section mentions which types of connectors the are compatible with the DSI inputs. They can use either the Hirose FX-type (which you highlighted) or the Samtec QSH-type connector and the part numbers are listed there.
The output port connector types are also listed in the "2.2 Connectors for DSI85 Output Ports" section.
So they can use the part numbers mentioned there to mate with the on-board connectors, or use a breakout board for testing (also listed).
Best regards,
Ikram