Part Number: DP83869HM
Tool/software:
Hi everyone, we have produced a prototype that implements the PHY DP83869HM.
For testing we have connected two of them in a back-to-back SGMII configuration.
The SGMII link is shown below:
After powering up, everything seems to be normal. All voltages rails are ok.
The PHY seem to work. LED TX/RX blinking and Link up LED lit.
However, the PC cannot detect any connection with the LAN network.
I am wondering if there is a mistake in the SGMII wiring or maybe it is a mistake in the bootstrapping.
I have used the bootstrapping depicted here:
mirroring is disabled