This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1021-Q1: Solution for ISO17987-7 chapter 5.2.5.3 acutal test result different from test report from TI

Part Number: TLIN1021-Q1


Tool/software:

Hello colleagues,

       We are designing an ECU include LIN transciver TLIN1021-Q1 for our customer. They EMC and electrical performance requirements standard required the test sample implement ISO-17987-7 chapter 5.2.5.3 test after finishing each test items. e,g, RE/CE/BCI/RI/ESD.

       When implement the 5.2.5.3 test, we found the test result(~120mV) not fulfill the standard requirements(≤20mV). Following are the actually test set-up and test result.  Please help to check our test set-up are correct or not, and tell the corrent setup.

      Besides the actual test setup  display in below, we also try method 2:change EN pin  to ground, method 3:change EN and Wake pin  to ground, while the result also ≥100mV, still keep a big distance from the ISO requirement.

       Above, thanks.

Figure 1: ISO-17987-7 chapter 5.2.5.3 requirement     

Figure 2 : test result from TI official test report 

Figure 3: the 3-rd EMC organization actual test setup                               

Figure 4: the 3-rd EMC organization actual test result (pink waveform)