This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: DS90UB947 and DS90UB940

Part Number: DS90UB947-Q1

Tool/software:

I have connected the DS90UB947 and DS90UB940 chips according to their respective datasheets. I want to connect the LVDS camera to the input and link the output to the Jetson Orin processor via CSI-2.

  1. Do I need to perform any programming in order to transfer the image?
  2. If programming is required, how can I access the drivers for the chips (DS90UB947 and DS90UB940)? My board has test points pulled up on the I2C lines of the chips.
  3. Additionally, do I need to connect the DS90UB947 to the Jetson processor via I2C?
  • Hi,

    1) The 940 doesn't require programming but here is an example of the 947 init code. 

    2) We do not provide drivers but we provide flat I2C logs. Please refer to the init file provided.

    3) Yes. 

    """
      TI Confidential - NDA Restrictions
    
      Copyright 2020 Texas Instruments Incorporated. All rights reserved.
    
      IMPORTANT: Your use of this Software is limited to those specific rights
      granted under the terms of a software license agreement between the user who
      downloaded the software, his/her employer (which must be your employer) and
      Texas Instruments Incorporated (the "License"). You may not use this Software
      unless you agree to abide by the terms of the License. The License limits your
      use, and you acknowledge, that the Software may not be modified, copied or
      distributed unless embedded on a Texas Instruments microcontroller which is
      integrated into your product. Other than for the foregoing purpose, you may
      not use, reproduce, copy, prepare derivative works of, modify, distribute,
      perform, display or sell this Software and/or its documentation for any
      purpose.
    
      YOU FURTHER ACKNOWLEDGE AND AGREE THAT THE SOFTWARE AND DOCUMENTATION ARE
      PROVIDED AS IS WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED,
      INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE,
      NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL TEXAS
      INSTRUMENTS OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT,
      NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER LEGAL
      EQUITABLE THEORY ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES INCLUDING BUT NOT
      LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT, PUNITIVE OR CONSEQUENTIAL
      DAMAGES, LOST PROFITS OR LOST DATA, COST OF PROCUREMENT OF SUBSTITUTE GOODS,
      TECHNOLOGY, SERVICES, OR ANY CLAIMS BY THIRD PARTIES (INCLUDING BUT NOT
      LIMITED TO ANY DEFENSE THEREOF), OR OTHER SIMILAR COSTS.
    
      Should you have any questions regarding your right to use this Software,
      contact Texas Instruments Incorporated at www.TI.com.
    
    """
    ############################
    # DS90UB947-Q1 Init Code Example v1.1
    # 947->948, Dual FPD-Link STP, 1920x1080@60Hz
    ############################
    
    import time
    import sys
    
    # System dependant variables - adjust according to system 
    UB947 = 0x18        # 947 I2C Address
    UB948 = 0x68        # Remote 948 Address
    StartAmbTemp = 25   # Example temperature measured by local sensor on PCB (Ambient temp around 947). In real system this should be read back from temp sensor during initialization 
    Hres = 1920         # Expected horizontal active resolution
    Vres = 1080         # Expected vertical active resolution 
    
    def pollstate():
        count=0
        board.WriteI2C(UB947,0x23,0x80)
        board.WriteI2C(UB947,0x24,0x80)
        mask = int('11111',2)
        state = board.ReadI2C(UB947,0x24,1)
        while (state & mask) != 27:   #27 = 5'b11011
            time.sleep(0.01)  #10ms delay
            state = board.ReadI2C(UB947,0x24,1)
            count = count +1
            if count == 10:
                print "Error: Serializer is not in Normal state"
                return(1)
        
        board.WriteI2C(UB947,0x23,0x0)
        board.WriteI2C(UB947,0x24,0x0)
    
            
    
    def initsequence():
    
        board.WriteI2C(UB947,0x03,0xDA) # Set I2C passthrough
        
        linked = 0
        retry = 0
        mask = int('10000000',2)
        while linked == 0:
            STS = board.ReadI2C(UB947,0x5A,1)
            if ((STS & mask) != 0):
                linked = 1
                print "Deserializer Detected"
            else:
                time.sleep(0.1)
                retry = retry + 1
                if retry == 10:
                    print "Error: No Deserializer Detected"
                    return()
    
        board.WriteI2C(UB948,0x4A,0x01) # Disable OLDI outputs on 948 to prevent screen glitches from appearing during the init process 
    
        ##### Init A Sequence
    
        # Errata #5 and 6
        board.WriteI2C(UB947,0x5B,0x03) # Force dual FPD-Link, disable reset on PLL frequency change 
    
        # Errata #10
        board.WriteI2C(UB947,0x16,0x02) # Adjust BCC watchdog timer to minimum
    
        # Errata #11
        board.WriteI2C(UB947,0x04,0x90) # Prevent AVMUTE for non-HDCP systems
    
    
    
        state_error = pollstate()  # Poll 947 state machine prior to applying init B errata
    
        if state_error == 1:
            return()
    
        ##### Init B Sequence 
    
        # # Errata #2 (only for older non-eFuse devices)
        # board.WriteI2C(UB947,0x40,0x10)
        # board.WriteI2C(UB947,0x41,0x4A)
        # board.WriteI2C(UB947,0x42,0x3F)
        # board.WriteI2C(UB947,0x41,0x4B)
    
        # if StartAmbTemp < 10:
        #     board.WriteI2C(UB947,0x42,0x88)
        # else:
        #     board.WriteI2C(UB947,0x42,0x89)
        # board.WriteI2C(UB947,0x41,0x49)
        # board.WriteI2C(UB947,0x42,0x10)
        # board.WriteI2C(UB947,0x42,0x00)
        # board.WriteI2C(UB947,0x40,0x14)
        # board.WriteI2C(UB947,0x41,0x4A)
        # board.WriteI2C(UB947,0x42,0x3F)
        # board.WriteI2C(UB947,0x41,0x4B)
        # if StartAmbTemp < 10:
        #     board.WriteI2C(UB947,0x42,0x88)
        # else:
        #     board.WriteI2C(UB947,0x42,0x89)
        # board.WriteI2C(UB947,0x41,0x49)
        # board.WriteI2C(UB947,0x42,0x10)
        # board.WriteI2C(UB947,0x42,0x00)
    
        # Errata #3 
        board.WriteI2C(UB947,0x40,0x10)
        board.WriteI2C(UB947,0x41,0x49)
        board.WriteI2C(UB947,0x42,0x16)
        board.WriteI2C(UB947,0x41,0x47)
        board.WriteI2C(UB947,0x42,0x20)
        board.WriteI2C(UB947,0x42,0xA0)
        board.WriteI2C(UB947,0x42,0x20)
        board.WriteI2C(UB947,0x42,0x00)
        board.WriteI2C(UB947,0x41,0x49)
        board.WriteI2C(UB947,0x42,0x00)
    
        time.sleep(0.01)
    
        ##### Timing Confirmation 
    
        retry = 0
        Hconfirm = 0
        Vconfirm = 0
        while (retry < 3):
            board.WriteI2C(UB948,0x68,0x08) # Enable PATGEN BIST
            time.sleep(0.1) # Critical time delay - do not adjust to a shorter value 
            board.WriteI2C(UB948,0x68,0x19) # H active High monitor
            Hhigh = board.ReadI2C(UB948, 0x69, 1)
            board.WriteI2C(UB948,0x68,0x09) # H active Low monitor
            Hlow = board.ReadI2C(UB948, 0x69, 1)
            board.WriteI2C(UB948,0x68,0x39) # V active High monitor
            Vhigh = board.ReadI2C(UB948, 0x69, 1)
            board.WriteI2C(UB948,0x68,0x29) # V active Low monitor
            Vlow = board.ReadI2C(UB948, 0x69, 1)
            board.WriteI2C(UB948,0x68,0x00) # Disable PATGEN BIST
    
            mask = int('00111111',2)
    
            hlowmask = Hlow & mask
            hhighmask = Hhigh & mask
            vlowmask = Vlow & mask
            vhighmask = Vhigh & mask
    
    
            hhighmask = hhighmask << 6
            vhighmask = vhighmask << 6
    
            Hactive = hhighmask | hlowmask
            Vactive = vhighmask | vlowmask
    
            if Hactive != Hres:
                retry  = retry + 1
                board.WriteI2C(UB947,0x40,0x10) # Reset OLDI PLL
                board.WriteI2C(UB947,0x41,0x49)
                board.WriteI2C(UB947,0x42,0x16)
                board.WriteI2C(UB947,0x41,0x47)
                board.WriteI2C(UB947,0x42,0x20)
                board.WriteI2C(UB947,0x42,0xA0)
                board.WriteI2C(UB947,0x42,0x20)
                board.WriteI2C(UB947,0x42,0x00)
                board.WriteI2C(UB947,0x41,0x49)
                board.WriteI2C(UB947,0x42,0x00)
                time.sleep(0.1)
            else:
                Hconfirm = 1
            if Vactive != Vres:
                retry  = retry + 1
                board.WriteI2C(UB947,0x40,0x10) # Reset OLDI PLL
                board.WriteI2C(UB947,0x41,0x49)
                board.WriteI2C(UB947,0x42,0x16)
                board.WriteI2C(UB947,0x41,0x47)
                board.WriteI2C(UB947,0x42,0x20)
                board.WriteI2C(UB947,0x42,0xA0)
                board.WriteI2C(UB947,0x42,0x20)
                board.WriteI2C(UB947,0x42,0x00)
                board.WriteI2C(UB947,0x41,0x49)
                board.WriteI2C(UB947,0x42,0x00)
                time.sleep(0.1)
            else:
                Vconfirm = 1
            if (Hconfirm == 1) and (Vconfirm == 1):
                break
    
        if (retry > 2):
            print "Error: Timing confirmation failed. Double check expected video resolution and OLDI video input"  
            return()
        else:
            print "Initialization Complete"
            board.WriteI2C(UB948,0x01,0x01) # Digital reset to restart AEQ 
            time.sleep(0.1) # Allow time for 948 to relock 
            board.WriteI2C(UB948,0x4A,0x00) # Enable OLDI outputs on 948
    
    initsequence()

    BR,

    Esther