Part Number: DP83TG720EVM-MC
Tool/software:
hi ,
I do not understand the Connection for LED0 and LED1 of the EVM What modes for dp83867 LED0 and LED1?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TG720EVM-MC
Tool/software:
hi ,
I do not understand the Connection for LED0 and LED1 of the EVM What modes for dp83867 LED0 and LED1?

Hi,
LED01 is pulled high by R94 so the pin is configured as an active low output. Meaning that when there is a link-up the LED01 pin is equal to GND.
LED11 is pulled low because it is separated from Vreg by the two diodes so it is configured as active high. When there is 1G bit data being transmitted LED11 is high and overcomes the forward voltage of the green diode to turn it on. When the signal is 100Mbit, LED11 is low and Vreg offers the voltage to enable the orange diode.
Best regards,
Nick
Hi ,
I don't thik so, both LED01and LED11 are configured as an active high, 100BASE-T link established: LED01 high LED11 low , enable the orange LED, 1000BASE-T link established: LED01 low LED11 high, enable the green LED。 I read the Register 0x0018 and 0x0019 ,they are configured 0x6156 and 0x0044.
but I have another question, LED01 is configured mode 3 and LED11 is configured mode 1?


Hi,
LED0 and LED1 are active high, LED2 is active low, as you have noticed in register 0x0018,
LED01 is configured mode 3 and LED11 is configured mode 1
This is correct.
Thanks,
David