Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB962-Q1: Recommended reflow profile

Part Number: DS90UB962-Q1

Tool/software:

Hello Expert,

Could you please provide following information regarding reflow profile?

1.1) Upper limit of peak temperature under reflow heat resistance condition (Ex : 260°C).

1.2) High temperature region holding temperature under reflow heat resistance condition (Ex : 230°C).

1.3) Upper limit of high-temperature region holding time under reflow heat resistance condition (Ex : 60 sec).

1.4) Number of reflows that the connector can support (Ex : Twice).

I think TI's standard reflow profile is as below.

https://www.ti.com/lit/an/spraby1a/spraby1a.pdf

However, there isn't answer for 1.4).
So I want to confirm it.

Best regards,
Kazuki Kuramochi