Part Number: TCA9509
Tool/software:
For the TC9509, we have the B side connected to 3.3V and the A side connected to 1.8V. During power on the 3.3V(side A) is powered up first. This 3.3V voltage rail is also connected to the EN signal. With the A side off and not yet powered, is it possible that the logic on the SCL/SDA side A could impact side B of the level shifter? We are concerned about potential leakage of the signal on the B side from the A side.