Part Number: DP83TC814R-Q1
Tool/software:
Hello TI Team,
We have used DP83TC814R-Q1 PHY with AM64xx CPU.
Our DTS Configuration looks like below:
&cpsw_port1 {
/*bootph-all;*/
status = "okay";
phy-mode = "rgmii-rxid";
phy-handle = <&cpsw3g_phy1>;
// fixed-link {
// speed = <100>;
// full-duplex;
// };
};
&cpsw3g_mdio {
bootph-all;
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&cpsw_mdio0_pins_default>;
cpsw3g_phy1: ethernet-phy@0 {
reg = <0x0>;
ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
// fixed-link {
// speed = <100>;
// full-duplex;
// };
};
};
With this configuration, we are able to see the CPSW is able to identify which PHY is connected. And link also we are able to detect.
root@am64xx:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 100baseT/Full
Supported pause frame use: Symmetric
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: Not reported
Advertised pause frame use: Symmetric
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: 100Mb/s
Duplex: Full
Auto-negotiation: off
master-slave cfg: forced slave
master-slave status: slave
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Supports Wake-on: d
Wake-on: d
Current message level: 0x000020f7 (8439)
drv probe link ifdown ifup rx_err tx_err hw
Link detected: yes
SQI: 7/7
If you can see the signal quality is also good, but we are not able to receive any packets.
root@am64xx:~# ethtool -S eth0
NIC statistics:
p0_rx_good_frames: 800
p0_rx_broadcast_frames: 169
p0_rx_multicast_frames: 631
p0_rx_crc_errors: 0
p0_rx_oversized_frames: 0
p0_rx_undersized_frames: 0
p0_ale_drop: 1
p0_ale_overrun_drop: 0
p0_rx_octets: 131103
p0_tx_good_frames: 0
p0_tx_broadcast_frames: 0
p0_tx_multicast_frames: 0
p0_tx_octets: 0
p0_tx_64B_frames: 0
p0_tx_65_to_127B_frames: 478
p0_tx_128_to_255B_frames: 144
p0_tx_256_to_511B_frames: 178
p0_tx_512_to_1023B_frames: 0
p0_tx_1024B_frames: 0
p0_net_octets: 131103
p0_rx_bottom_fifo_drop: 0
p0_rx_port_mask_drop: 1
p0_rx_top_fifo_drop: 0
p0_ale_rate_limit_drop: 0
p0_ale_vid_ingress_drop: 0
p0_ale_da_eq_sa_drop: 0
p0_ale_block_drop: 0
p0_ale_secure_drop: 0
p0_ale_auth_drop: 0
p0_ale_unknown_ucast: 0
p0_ale_unknown_ucast_bytes: 0
p0_ale_unknown_mcast: 0
p0_ale_unknown_mcast_bytes: 0
p0_ale_unknown_bcast: 0
p0_ale_unknown_bcast_bytes: 0
p0_ale_pol_match: 0
p0_ale_pol_match_red: 0
p0_ale_pol_match_yellow: 0
p0_ale_mcast_sa_drop: 0
p0_ale_dual_vlan_drop: 0
p0_ale_len_err_drop: 0
p0_ale_ip_next_hdr_drop: 0
p0_ale_ipv4_frag_drop: 0
p0_tx_mem_protect_err: 0
p0_tx_pri0: 0
p0_tx_pri1: 0
p0_tx_pri2: 0
p0_tx_pri3: 0
p0_tx_pri4: 0
p0_tx_pri5: 0
p0_tx_pri6: 0
p0_tx_pri7: 0
p0_tx_pri0_bcnt: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri2_bcnt: 0
p0_tx_pri3_bcnt: 0
p0_tx_pri4_bcnt: 0
p0_tx_pri5_bcnt: 0
p0_tx_pri6_bcnt: 0
p0_tx_pri7_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri1_drop: 0
p0_tx_pri2_drop: 0
p0_tx_pri3_drop: 0
p0_tx_pri4_drop: 0
p0_tx_pri5_drop: 0
p0_tx_pri6_drop: 0
p0_tx_pri7_drop: 0
p0_tx_pri0_drop_bcnt: 0
p0_tx_pri1_drop_bcnt: 0
p0_tx_pri2_drop_bcnt: 0
p0_tx_pri3_drop_bcnt: 0
p0_tx_pri4_drop_bcnt: 0
p0_tx_pri5_drop_bcnt: 0
p0_tx_pri6_drop_bcnt: 0
p0_tx_pri7_drop_bcnt: 0
rx_good_frames: 0
rx_broadcast_frames: 0
rx_multicast_frames: 0
rx_pause_frames: 0
rx_crc_errors: 0
rx_align_code_errors: 0
rx_oversized_frames: 0
rx_jabber_frames: 0
rx_undersized_frames: 0
rx_fragments: 0
ale_drop: 0
ale_overrun_drop: 0
rx_octets: 0
tx_good_frames: 27
tx_broadcast_frames: 0
tx_multicast_frames: 27
tx_pause_frames: 0
tx_deferred_frames: 0
tx_collision_frames: 0
tx_single_coll_frames: 0
tx_mult_coll_frames: 0
tx_excessive_collisions: 0
tx_late_collisions: 0
rx_ipg_error: 0
tx_carrier_sense_errors: 0
tx_octets: 3732
tx_64B_frames: 0
tx_65_to_127B_frames: 15
tx_128_to_255B_frames: 12
tx_256_to_511B_frames: 0
tx_512_to_1023B_frames: 0
tx_1024B_frames: 0
net_octets: 3732
rx_bottom_fifo_drop: 0
rx_port_mask_drop: 0
rx_top_fifo_drop: 0
ale_rate_limit_drop: 0
ale_vid_ingress_drop: 0
ale_da_eq_sa_drop: 0
ale_block_drop: 0
ale_secure_drop: 0
ale_auth_drop: 0
ale_unknown_ucast: 0
ale_unknown_ucast_bytes: 0
ale_unknown_mcast: 0
ale_unknown_mcast_bytes: 0
ale_unknown_bcast: 0
ale_unknown_bcast_bytes: 0
ale_pol_match: 0
ale_pol_match_red: 0
ale_pol_match_yellow: 0
ale_mcast_sa_drop: 0
ale_dual_vlan_drop: 0
ale_len_err_drop: 0
ale_ip_next_hdr_drop: 0
ale_ipv4_frag_drop: 0
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 0
tx_mem_protect_err: 0
tx_pri0: 27
tx_pri1: 0
tx_pri2: 0
tx_pri3: 0
tx_pri4: 0
tx_pri5: 0
tx_pri6: 0
tx_pri7: 0
tx_pri0_bcnt: 3732
tx_pri1_bcnt: 0
tx_pri2_bcnt: 0
tx_pri3_bcnt: 0
tx_pri4_bcnt: 0
tx_pri5_bcnt: 0
tx_pri6_bcnt: 0
tx_pri7_bcnt: 0
tx_pri0_drop: 0
tx_pri1_drop: 0
tx_pri2_drop: 0
tx_pri3_drop: 0
tx_pri4_drop: 0
tx_pri5_drop: 0
tx_pri6_drop: 0
tx_pri7_drop: 0
tx_pri0_drop_bcnt: 0
tx_pri1_drop_bcnt: 0
tx_pri2_drop_bcnt: 0
tx_pri3_drop_bcnt: 0
tx_pri4_drop_bcnt: 0
tx_pri5_drop_bcnt: 0
tx_pri6_drop_bcnt: 0
tx_pri7_drop_bcnt: 0
root@am64xx:~# ifconfig eth0 192.168.3.11 up
root@am64xx:~# ifconfig eth0
eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500
inet 192.168.3.11 netmask 255.255.255.0 broadcast 192.168.3.255
inet6 fe80::2ab5:e8ff:fecf:ec59 prefixlen 64 scopeid 0x20<link>
ether 28:b5:e8:cf:ec:59 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 34 bytes 4776 (4.6 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
root@am64xx:~# ping 192.168.3.10
PING 192.168.3.10 (192.168.3.10): 56 data bytes
^C
--- 192.168.3.10 ping statistics ---
2 packets transmitted, 0 packets received, 100% packet loss
root@am64xx:~# ethtool -S eth0
NIC statistics:
p0_rx_good_frames: 845
p0_rx_broadcast_frames: 181
p0_rx_multicast_frames: 664
p0_rx_crc_errors: 0
p0_rx_oversized_frames: 0
p0_rx_undersized_frames: 0
p0_ale_drop: 1
p0_ale_overrun_drop: 0
p0_rx_octets: 138698
p0_tx_good_frames: 0
p0_tx_broadcast_frames: 0
p0_tx_multicast_frames: 0
p0_tx_octets: 0
p0_tx_64B_frames: 6
p0_tx_65_to_127B_frames: 496
p0_tx_128_to_255B_frames: 153
p0_tx_256_to_511B_frames: 190
p0_tx_512_to_1023B_frames: 0
p0_tx_1024B_frames: 0
p0_net_octets: 138698
p0_rx_bottom_fifo_drop: 0
p0_rx_port_mask_drop: 1
p0_rx_top_fifo_drop: 0
p0_ale_rate_limit_drop: 0
p0_ale_vid_ingress_drop: 0
p0_ale_da_eq_sa_drop: 0
p0_ale_block_drop: 0
p0_ale_secure_drop: 0
p0_ale_auth_drop: 0
p0_ale_unknown_ucast: 0
p0_ale_unknown_ucast_bytes: 0
p0_ale_unknown_mcast: 0
p0_ale_unknown_mcast_bytes: 0
p0_ale_unknown_bcast: 0
p0_ale_unknown_bcast_bytes: 0
p0_ale_pol_match: 0
p0_ale_pol_match_red: 0
p0_ale_pol_match_yellow: 0
p0_ale_mcast_sa_drop: 0
p0_ale_dual_vlan_drop: 0
p0_ale_len_err_drop: 0
p0_ale_ip_next_hdr_drop: 0
p0_ale_ipv4_frag_drop: 0
p0_tx_mem_protect_err: 0
p0_tx_pri0: 0
p0_tx_pri1: 0
p0_tx_pri2: 0
p0_tx_pri3: 0
p0_tx_pri4: 0
p0_tx_pri5: 0
p0_tx_pri6: 0
p0_tx_pri7: 0
p0_tx_pri0_bcnt: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri2_bcnt: 0
p0_tx_pri3_bcnt: 0
p0_tx_pri4_bcnt: 0
p0_tx_pri5_bcnt: 0
p0_tx_pri6_bcnt: 0
p0_tx_pri7_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri1_drop: 0
p0_tx_pri2_drop: 0
p0_tx_pri3_drop: 0
p0_tx_pri4_drop: 0
p0_tx_pri5_drop: 0
p0_tx_pri6_drop: 0
p0_tx_pri7_drop: 0
p0_tx_pri0_drop_bcnt: 0
p0_tx_pri1_drop_bcnt: 0
p0_tx_pri2_drop_bcnt: 0
p0_tx_pri3_drop_bcnt: 0
p0_tx_pri4_drop_bcnt: 0
p0_tx_pri5_drop_bcnt: 0
p0_tx_pri6_drop_bcnt: 0
p0_tx_pri7_drop_bcnt: 0
rx_good_frames: 0
rx_broadcast_frames: 0
rx_multicast_frames: 0
rx_pause_frames: 0
rx_crc_errors: 0
rx_align_code_errors: 0
rx_oversized_frames: 0
rx_jabber_frames: 0
rx_undersized_frames: 0
rx_fragments: 0
ale_drop: 0
ale_overrun_drop: 0
rx_octets: 0
tx_good_frames: 39
tx_broadcast_frames: 3
tx_multicast_frames: 36
tx_pause_frames: 0
tx_deferred_frames: 0
tx_collision_frames: 0
tx_single_coll_frames: 0
tx_mult_coll_frames: 0
tx_excessive_collisions: 0
tx_late_collisions: 0
rx_ipg_error: 0
tx_carrier_sense_errors: 0
tx_octets: 5598
tx_64B_frames: 6
tx_65_to_127B_frames: 15
tx_128_to_255B_frames: 15
tx_256_to_511B_frames: 3
tx_512_to_1023B_frames: 0
tx_1024B_frames: 0
net_octets: 5598
rx_bottom_fifo_drop: 0
rx_port_mask_drop: 0
rx_top_fifo_drop: 0
ale_rate_limit_drop: 0
ale_vid_ingress_drop: 0
ale_da_eq_sa_drop: 0
ale_block_drop: 0
ale_secure_drop: 0
ale_auth_drop: 0
ale_unknown_ucast: 0
ale_unknown_ucast_bytes: 0
ale_unknown_mcast: 0
ale_unknown_mcast_bytes: 0
ale_unknown_bcast: 0
ale_unknown_bcast_bytes: 0
ale_pol_match: 0
ale_pol_match_red: 0
ale_pol_match_yellow: 0
ale_mcast_sa_drop: 0
ale_dual_vlan_drop: 0
ale_len_err_drop: 0
ale_ip_next_hdr_drop: 0
ale_ipv4_frag_drop: 0
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 0
tx_mem_protect_err: 0
tx_pri0: 39
tx_pri1: 0
tx_pri2: 0
tx_pri3: 0
tx_pri4: 0
tx_pri5: 0
tx_pri6: 0
tx_pri7: 0
tx_pri0_bcnt: 5598
tx_pri1_bcnt: 0
tx_pri2_bcnt: 0
tx_pri3_bcnt: 0
tx_pri4_bcnt: 0
tx_pri5_bcnt: 0
tx_pri6_bcnt: 0
tx_pri7_bcnt: 0
tx_pri0_drop: 0
tx_pri1_drop: 0
tx_pri2_drop: 0
tx_pri3_drop: 0
tx_pri4_drop: 0
tx_pri5_drop: 0
tx_pri6_drop: 0
tx_pri7_drop: 0
tx_pri0_drop_bcnt: 0
tx_pri1_drop_bcnt: 0
tx_pri2_drop_bcnt: 0
tx_pri3_drop_bcnt: 0
tx_pri4_drop_bcnt: 0
tx_pri5_drop_bcnt: 0
tx_pri6_drop_bcnt: 0
tx_pri7_drop_bcnt: 0
If you look at the dts configuration we have kept fixed link mode configuration at 2 places. We tried to configure at respective place as well as at both place, but it is not working.
Kindly share some insights what can be changed to get this working.
With regards,
Anuj Shah