This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90C385A: Error in IBIS file

Part Number: DS90C385A

Tool/software:

Hello, I am trying to do a design using a DS90C385AMT/NOPB LVDS transmitter. When I select the IBIS model available at DS90C385A data sheet, product information and support | TI.com it does not compile because of the following errors:

ERROR - Model DS90C385_OUT: The [Rising Waveform] 
      with [R_fixture]=50 Ohms and [V_fixture]=0V
      has TYP column DC endpoints of  0.00V and  1.41v, but
      an equivalent load applied to the model's I-V tables yields
      different voltages ( 0.00V and  0.19V),
      a difference of  0.18% and 625.42%, respectively.
ERROR - Model DS90C385_OUT: The [Falling Waveform] 
      with [R_fixture]=50 Ohms and [V_fixture]=0V
      has TYP column DC endpoints of  1.00V and  1.41v, but
      an equivalent load applied to the model's I-V tables yields
      different voltages ( 0.00V and  0.19V),
      a difference of 515.31% and 625.73%, respectively.

Errors  : 2

File Failed

I would deeply appreciate if you could update the model with the respective corrections.