This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822H: DP83822

Part Number: DP83822H

Tool/software:

I am integrating the DP83822 Ethernet PHY with a Renesas RX72N microcontroller on a custom board using the RMII interface. The PHY reset sequence is executed properly, and the RESET_N pin goes high as expected. However, I am unable to read any register values from the DP83822 using the MDIO/MDC interface. 

Hardware Details:

  • MCU: Renesas RX72N

  • PHY: Texas Instruments DP83822

  • Interface: RMII (Reference Clock: 25MHz Crystal)

  • Power Supply: 3.3V (Checked and stable)

  • Connections:

    • MDC (PHY) <-> MDC (RX72N)

    • MDIO (PHY) <-> MDIO (RX72N) 

    • RESET_N (PHY) <-> MCU GPIO (Driven High after 10ms delay post-power-up)

  • Hi,

    Are you able to show the DP83822 schematic? I can check this to ensure there are no issues with your MDC/MDIO implementation.

    If you'd like to share this privately, please accept my friendship request and use the 'direct message' feature on E2E. This will open a separate space that is only viewable by you and I.

    Best,

    Shane

  • Hi Shantanu,

    Seeing as we have taken this conversation to private message, I'll resolve our E2E thread here.

    You can continue to reply here or in our private message and I will respond.

    Best,

    Shane