Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3630A:I2C driver for Windows HID interface

Part Number: LM3630A
Other Parts Discussed in Thread: LM3630

Tool/software:

I would like to ask if there is a Windows driver available for the LM3630A.

Currently, I’m trying to connect the LM3630 to an Intel SoC via I2C,

but it seems I can’t control the LM3630 using the Android-based method.

The customer mentioned that a driver under HID is required for it to function properly on Windows.

Could you provide the driver or any reference code for implementation?

thank you