Part Number: SN75LVCP600S
Other Parts Discussed in Thread: DS100BR210, SN75LVCP600
Tool/software:
Hi,
For some reason, I have to choose a part number, but I am actually looking for a recommendation.
I’m using a repeater (89HP0604Q IDT) and am looking for a replacement.
The data rate is a maximum of 6Gbps, coming from a 5m cable.
I need an IC that can operate without I2C (resistor straps).
The package size has to be a maximum of 3x6.5mm.
Two channels are preferred.
The same part number will be used for both the receiver and transmitter.
Please help me find an appropriate IC.
Thanks.