Part Number: AM26LV31
Tool/software:
I have of two these drivers on the same board close together running at 3.3V. Inputs are 0/3.3 signals. The “Z” sides of the differential outputs when measured to GND show 3.3V signals but the “Y” sides all have 2Vdc, no matter what the input. This is the same for both chips and all 8 signals.
This is not the first build so this board has worked in other units, but the current location prevents me from checking the G and Gbar logic inputs. Is there a configuration of G/Gbar that would cause this or other configuration issues that might drive 2V on all the “Y” pins.