Part Number: SN55LVDS32
Tool/software:
Hello,
I'm working with SN55LVDS32 in a bus configuration in which I need to measure the bus itself. It's difficult to find a buffer that meets reliability qualifications, has enough bandwidth, and has a low enough bias current to sense the bus such that when disconnected the open-circuit fail safe is still functional. I've seen the app-note on terminations, but did not see anything about adding external pull-ups to 'strengthen' the overall pull-ups provided within.
Would adding an external pair of 300 kOhm resistors as pull ups to VCC have negative effects on bandwidth or other parameters?
Thank you,
Scott Foley