Part Number: DS90UB971-Q1
Tool/software:
Hi,
Please help to review DS90UB971 schematic as following, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB971-Q1
Tool/software:
Hi,
Please help to review DS90UB971 schematic as following, thanks.
Hi Che,
I can review and will get back to you by beggining of next week
Hello Che,
here is my review feedback.
- Make sure the CSI traces are 100-ohm differential and length matched.
- Make sure I2C pins are pulled up as per Table 6-12
- Make sure both DOUT AC-coupling caps have the same voltage rating (50V)
- LPF1 requires a 1.8nF cap not 2.2nF
- On the power-supply pins (VDD_1P8_xx) our recommendation is to use 10uF caps not 1uF. Refer to Figure 7-3