Part Number: LMH1297EVM
Other Parts Discussed in Thread: LMH1297
Tool/software:
The LMH1297EVM User's Guide mentions on page 5:
5.1 Modes of Operation
The LMH1297EVM can be used in one of three modes:
1. Pin Mode (Default) – Provides general access to the LMH1297 signal integrity and I/O control settings
with IC pin-level logic.
2. SPI Mode – Provides full access to the LMH1297 signal integrity and control settings with MISO,
MOSI, SCK, and SSN pins.
3. SMBus Mode – Provides full access to the LMH1297 signal integrity and control settings with SDA,
SCL, and GND pins. ADDR0 and ADDR1 pins are used for SMBus address strap.
The LMH1297 datasheet then has the following table for the MODE_SEL pin on page 25:

This chart only specifies how to set SPI Mode or SMBus Mode.
It is not clear how to activate the Pin Mode.
So my question is, how do you activate the default Pin Mode?