Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PR410: SIGCON for DS160PR410

Part Number: DS160PR410

Tool/software:

Hello,

I would like to use the SIGCON tool to create an EEPROM file or modify it for DS160PR410. Which version do I download from this tool below? For Linux and Windows.

https://www.ti.com/tool/SIGCONARCHITECT

Do I need a paid version of NI labview? If not which one do I use there?

Also, I am using the master mode and am connected to one EEPROM AT24C02C-SSHM-B with I2C address 0x50 (0xA0, 0xA1).

Divakar

  • Hello Divakar,

    Please use the SIGCONARCHITECT3-WRTE installer, which will install both the needed LabView 2016 runtime engine and the SigCon Architect GUI.

    The EEPROM address of 0x50 (0xA0/0xA1) is supported by the DS160PR410 GUI profile. This can be requested through the DS160PR410's More information 'request' button on the product page.

    Best,
    David