Part Number: DS280MB810
Other Parts Discussed in Thread: DS560MB410
Tool/software:
Hello,
I consider using the DS280MB810 as a de-mux device, in a 100GBase-KR interface design.
The de-mux is required in a midplane scenario, so the link between one side can be switched between 2 selectable
paths (similar to a redundancy scheme).
The most critical feature is transparency so signal characteristics through DS280MB810 is preserved for each of the
de-muxed selected options – so link training is performed between both link sides, whatever de-mux option is selected.
A total bypass would seem to be required to enable the mentioned transparency, however according to datasheet,
It seems that the "bypass" option only bypasses boost stage 1, while the signal is driven via boost stage 2.
Datasheet states that "…EQ boost stage 2 controls. Directly goes to analog. No override bit is needed…" but it is not clear
why the bypass doesn't include Boost stage 2 as well.
There seems to be also DS560MB410 device as option, would that be more suitable for the described application?
Best Regards,
Arie Menscher