Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7340: TUSB7340 question

Part Number: TUSB7340

Tool/software:

We are planning to design in TUSB7340 bridge to extend USB port slot number.

Some questions need to be clarified.

1. Where can I find demo board ordering page?

2. Is TUSB7340 belong NRND part?

3. From demo board schematics, there is a 1Kb EEPROM.

    What parameter should be stored in it?

    Is it need to pre-program before SMT production or it could be store setting in production test? 

4. If we have a 4-port USB hub(2.0/3.0) IC connect to TUSB7340, the consumption could reach as low as idle 79mW by SW setting? 

5. Data sheet lack of USB2.0*1 consumption, do you have entire consumption data?