Tool/software:

What might be the possible reasons? Can it be improved by configuring the corresponding registers?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:

What might be the possible reasons? Can it be improved by configuring the corresponding registers?
Hi,
As these are system level tests, I suggest taking a look at the implementation of the CSI-2 traces.
Below are layout guidelines for CSI-2 available in the UB960 datasheet:

Secondly, we recommend checking the VDD18 rails on the UB960 to confirm the rails are within specification of VDD18 with voltage 1.8V +/-10% and no more than 25mVpp noise.
Best,
Zoe
Hello,
Happy to help. I will close this thread for the time being. The thread can be reopened by providing another response.
Best,
Zoe