Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS16EV5110A: Vocm Explanation

Part Number: DS16EV5110A

Tool/software:

The data sheet gives the CML output Vocm as Vdd-0.3 to Vdd-0.2 and Vo differential swing as 800mV - 1200mV p-p.  At 3.3V Vdd, that means measuring single ended Vo could be 3.1V ocm + 0.6V = 3.7V max which is above Vdd.  Wouldn't it clamp at Vdd and cause an assymetric signal?  What am I misunderstanding?