Part Number: TMDS181
Tool/software:
Hi David,
Per talked, please help to give some debug direction asap, there are 3 key projects share the same base board that using TMDS181, this issue has blocked the progress of customer project. As this board is in TI Lab, can we try to reproduce in TI Lab? Thanks!
The issue behavior:
HDMI 4K did not display after multiple plugging and unplugging, and 4K did not display after waking up from sleep.
The sch:8546.HDMI Re-timer 线路12.24.pdf Also, modified the Vsadj, choke selection, EQ_SEL like we recommend.
The HPD_SRC, HPD, 3.3V, 1.8V when the abnormality occurred:
HPD:

Sleep HPD:

Sleep wake:

BRs,
Rannie