This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044A: Hub appears to put terminations on downstream pins when there is no upstream partner for SS, causing downstream devices to mis-behave

Part Number: TUSB8044A


Tool/software:

HI I'm currently debugging an issue where it appears that the hub is putting termination on the downstream port SS pins when there is no upstream SS partner. 

The signal chain looks like this TUSB8044A ->TUSB5522PI->TMUXHS4446->Type-c Connector.  Would any of these give a false positive to the hub for it to think there is an upstream partner?  What conditions would cause the hub to put downstream terminations if there are no upstream connection?  

The hub is not generating LFPS pings or jumping into compliance mode, but the downstream device is.

What is happening is on port 4 there is a Realtek RTL8153B connected, it is jumping into compliance mode and not enumerating usb 2.0.  The host device is an iPad 10th gen which is USB2.0 only.  A USB 2.0 mouse will always work.  

Thanks,