Part Number: DS90UB913A-Q1
Other Parts Discussed in Thread: DS90UB960-Q1, DS90UB954-Q1, , DS90UB933-Q1, DS90UB960-Q1EVM
Tool/software:
I'm spshin of Unitrontech
We are currently developing a system that supports 12−bit parallel cameras using the DS90UB913A serializer.
According to the datasheet, the DS90UB913A accepts 10- or 12-bit parallel input and serializes the data.
It also states compatibility with deserializers that output MIPI CSI-2, such as the DS90UB960. Our application processor (AP) only supports MIPI CSI-2 input.
Therefore, we would like to confirm whether the following configuration is supported and works as expected:
Parallel input to DS90UB913A → FPD-Link III → Deserializer (e.g., DS90UB960-Q1 or DS90UB954-Q1) → MIPI CSI-2 output to the AP.
Could you please confirm if this configuration is valid and operational?