Part Number: SN65HVD230
Other Parts Discussed in Thread: TCAN3414
Tool/software:
Hey Friends at TI,
I am trying to create a CAN communication system with the SN65HVD230. To design the system, I have taken reference from some online guides [1], [2] and SN65VHD230 datasheet to design a robust CAN system. Although I have a question with the implementation I did.
Below is the circuit for your reference:
I fear that If there is a constant biased voltage of let's say 42V given on the CAN lines the TVS will go into the avalanche breakdown mode and short the voltage to ground, in which case my device would still be safe but the device providing 42V will be shorted.
With this fear in mind i plan on putting a fuse on each line, which in that particular case will protect the other device too.
- Does putting fuse on these lines have any repercussions that I don't know of?
- How many amps of fuse is required on the line? (I assume a 250mA fuse would be very much more than fine too)
- From the look at the schematic, do you guys have any other suggestions for the overall implementation?
Thanks,
Shlok Desai