This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL16C754B interrupt signals

The data sheet states in Terminal Descriptions on page 3 that INTA-D are the interrupt lines.  The description in the Modem Control Register on page 29 (Table 12) appears to refer to these as IRQ(A-D).  In Table 8 on page 26, MCR bit 3 is labeled "IRQ Enable."  Are the INT / IRQ designators all for the same signals?  This is potentially confusing.

There is also reference to signals IRQ3-IRQ15, DRO0, DRO1, and DRO3 in Note 9 on page 18 - this is the only mention of these signals, so the note really doesn't seem to make much sense for this part.

One more question: should a weak pulldown be used on the INTA-D signals for the case in which they might be disabled so as not to leave them floating?

  • Hi Peter,

    INT and IRQ are used somewhat interchangeably in the datasheet. The lines should be referred to as INTA-INTD in the datasheet. The reference to IRQ is based on the original PC standard interrupt request signals and I am not sure why that carried over to our datasheet. Table 8 should refer to "INT Enable" and not "IRQ Enable". The modem control register should also refer to these signals as INTA-INTD.

    Note 9 on page 18 should also refer to INTA-INTD. I'm not sure why the PC interrupts IRQ3-IRQ15 are referenced. I do not know what DRO1 - DRO3 signals are.

    INTA-INTD are outputs and do not require a weak pull-down resister if they are not connected to the processor interrupts.

    Thank you for pointing out the inconsistency. I will submit the changes to the technical documentation team.

    Best Regards,

    Joe

  • Peter,

    The changes have been submitted to technical documentation services.

    Best Regards,

    Joe