This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3221: Are Rout are HighZ when chip is in Auto-power-down state?

Part Number: MAX3221

Tool/software:

Hi there.

I would like to use the MAX3221CPWR chip on my circuit.

I have a UART input OR an RS232 input connected to the PCB (not at the same time) which communicate with other hardware via an RS485 chip.

The Rout output would be interference with the UART input, if the RoutDriver would not be disable on Auto-power-down state.

I cant find any information about that in the datasheet, but i have to know it exactly.

Otherwise i have to decouple the two signal paths additionaly.

Thank you in advance!