Other Parts Discussed in Thread: TLV1811, TLV1871, GD65232
Tool/software:
Hello, and thank you in advance for your help.
I'm writing to see if it's OK to power the V+ and V- rails of the TRS202E with an external +12V / -12V power source. I would leave out the charge pump capacitors (C1 and C2 in the datasheet). It's a long story as to why I prefer to do this, glad to bore you with it if you like. It seems almost implied from the datasheet that this is OK, but I want to check with you first.
Thanks,
David Stadille